Main Application Window

Upon successful login, the main application window is displayed. This window is divided into three sections: Application Header; main Menu; and Main Area, which is part of the main Menu.

Application Header

This header displays the number of active alarms after you click a badge, the application navigates to the Insights summary. It also provides access to a personal user profile and logout button.

Main Menu

The main menu provides access to all application options. A selection in this menu populates the Main Area with applicable information.

Main Area

The main area displays information according to the option selected in the Main Menu.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?