Add Work Location Name to Component Tables (Optional)
In addition to pushing the Work Location itself, you can also choose to store the Work Location Name within the components’ tables. For example, if you push a structure back to the GIS, the structure’s attribute table can include its Work Location Name.
-
Every Work Location has two names: Work Location Name and Work Location Short Name.
-
You can choose one name to push back to the GIS, but you cannot push both.
To map the Work Location Name or Short Name to the components’ tables, follow these steps:
-
In Solution Center > Designer > Catalog, click Electric GIS Schema or Gas GIS Schema.
-
Ensure the Schema drop-down is set to Tables.
-
Click the component you want to configure.
-
Map either the WorkLocationName or WorkLocationShortName to an appropriate GIS field such as WorkLocationID.
-
Check “Push to GIS” for the name field.
-
Uncheck “Import” for the name field. Importing Work Location fields is not currently supported.
-
-
Click Save.
-
Repeat for other desired components.
-
Restart the Edge Service to see the changes reflected in the Designer XI application.