ArcFM Web XI

ArcFM Web is an intuitive, powerful, and lightweight application that expands the power of targeted web-mapping applications throughout your organization and maximizes the possibilities of GIS for use anytime, anywhere, on any device. As a web-based application, ArcFM Web’s HTML5/JavaScript technology provides effortless interaction with your organization’s data. ArcFM Web maximizes your investment in ArcGIS Server, ArcGIS Online, and Portal for ArcGIS web-mapping technologies. The value of ArcFM Web is from the partnership with VertiGIS (formerly Latitude Geographics). We leverage the VertiGIS Studio Web product to provide a comprehensive web viewer on the ArcGIS platform. Additionally, ArcFM Web exists inside your own environment, mostly on your Portal for ArcGIS machines.

We provide you with an ArcFM Web environment. To create a Web environment, contact the License Manager and provide your company’s contact information plus initial licensing requirements (product name: ArcFM Web; Start Date and End Date). The License Manager works closely with VertiGIS to set up your tenant and quickly give you the required access.

Once your environment is set up, all your access questions can be answered through myArcFM under the Log a Case. License contracts are updated accordingly at contract renewals. Any overuse of licenses is taken into account at contract renewal.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?