Cables

When you locate or select a cable, Wavepoint displays two tabs in the left pane: Details and Fibers.

  • Do you not see the Details and Fibers tabs?

    • Most likely, you have selected the cable on the map, but have not yet clicked the cable name to further open it and see its internal information.

    • Click the cable name once, and the application displays the Details and Fibers tabs.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?