Details

This tab provides detailed information about the cable, including its start and end points and high-level attributes. You can see the start and end points labeled on the map, and you can also click the start and end points on the Details tab to view more information about them.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?