Device Locations

This topic pertains to device locations that are fiber components with a physical point on the map. They are most typically a terminating location in the network to which service is provided.

In your GIS data model, devices might also be modeled as non-spatial tables that are related to spatial features such as patch locations or splices. If so, you find information about such devices by locating the parent, physical patch location or splice.

After locating a physical device, Wavepoint provides two tabs: Details and Inside.

  • Do you not see the Details and Inside tabs?

    • Most likely, you have selected the device on the map, but have not yet clicked the name to further open it and see its internal information.

    • Click the name once, and the application displays the Details and Inside tabs.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?