Distance

To measure the linear distance between two or more points, click the Distance Measurement   tool, then click once on the map to start the measurement:

  • If you want to measure between two points, double-click at the endpoint.

  • If you want to measure between more than two points, continue single clicking in the map, and double-click at the endpoint to stop the measurement.

    TIP: You can still zoom and pan the map while measuring. To pan, click and hold to drag the map into position.
  • After double-clicking, that sequence of measurement is over. To start a new measurement, click once somewhere on the map.

  • Click the unit of measure drop-down to change the unit of measure.

  • View a running total of the distance being measured under Measurement Result:

To stop measuring, click the Distance Measurement tool to toggle it off.


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?