Fibers

The Fibers tab displays information about the strands that belong to the cable, as well as their availability status.

The Fibers tab displays information about the strands that belong to the cable, as well as their circuit information and availability status. Wavepoint provides the ability to view multiple circuits for one fiber.

TIP: To locate a particular strand, either scroll through the list or use the Find tool in your web browser (Ctrl+F).

If the cable uses a buffer tube > strand arrangement, the tab displays the buffer tube color first followed by the fiber strand color:

If the cable uses a bundle > ribbon > strand arrangement, the tab displays the bundle color, then the ribbon color, and finally the fiber strand color:

Click a fiber link to run a trace on a fiber strand.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?