Full Path Trace from a Port

A trace can be initiated from any port on any kind of device or panel.
  1. Locate the desired rack, device, or splitter.
  2. On the Ports tab, locate the desired port and click it.

  3. On the left-hand side, specify Full Path and optionally a specific wavelength, then click Trace.

  4. Much like the Fiber Connectivity trace, the Details tab provides summary information, and the Path tab provides a one-line diagram of the trace results.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?