Inside

The Inside tab contains a list of devices at that location.

Click the name of the device to view its attributes and see a visualization of the device itself.

The Details tab appears in the left pane with more information about the device. To the right, the Ports tab contains the representation of the device.

After clicking the device, you can:

  • Use your mouse cursor to pan around the device.

  • Hover over a port to view more information including type, status, and circuits.

When you click a port, the left pane displays the same details for the port including type, status, and circuits.

After clicking a port, you can:

  • Run a Full Path Trace with or without a wavelength filter.

  • Run an OTDR Trace with a distance.

  • If present, click the circuit name to see details and extent of that circuit.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?