Trace

Wavepoint provides several ways to trace the fiber network. You can trace fiber connectivity, with or without a designated circuit. You can run Full Path and OTDR traces from ports and splice points. Further, you can run a trace through a splitter, and you have the opportunity to direct the trace path on the input or output side of the splitter. All traces provide summary details of the results and a one-line diagram of the trace path. Finally, all this information can be printed, including the diagrams.

IMPORTANT: Regarding any trace below, if after the trace you receive the error message, “Error loading trace data: The underlying connection was closed: An unexpected error occurred on a receive,” the most likely reason is that the fiber data is not converted to use ArcFM Objects. While unlikely, this can occur if - at a company level - your GIS data was migrated or the fiber network was rebuilt. Have an administrator visit the Configuration Guide topic Verify Fiber Data is Converted to Use ArcFM Objects to investigate.


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?