Trace through a Splitter

When a trace encounters a splitter, it initially stops at the splitter device and displays the various output paths emanating from that point forward. You can then click the desired output port to continue the trace along that path. The trace starts like the ones described above:
  1. Locate and click the desired port or fiber to initiate the trace.
  2. When the trace encounters a splitter, it pauses the trace and displays the splitter in both the one-line diagram and on the map. Further, it displays the possible input and output ports on the diagram and their immediate cable connections on the map. For example, in this image, notice the trace has temporarily stopped at a 1 x 4 splitter, and there are two possible paths (on the map) from that device.

  3. To continue the trace, click the desired input or output port. For example, in the following image output port 1 was chosen, and the trace continued along that path.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?