Trace through an Interleave (Multi-Inport) Splitter

When you trace through an interleave (multi-inport) splitter, the steps are the same as above. The only difference is that when the trace arrives at a branch point, it is noted in the one-line diagram.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?