How do I add a node cabinet to existing stranding?

DHFC does not allow for inserting a structure on an existing (imported or placed) section of strand, whether it be underground or overhead. You can, however, set an underground structure type to node cabinet, assuming that Designer HFC Catalog is configured with that structure type. Additionally, you can use the Place Strand  tool to add the structure and link it to existing stranding.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?