Coded Value Domain to Support Plugins

Conditioning taps and inline equalizers (LEQ/RC) can be coupled with a variety of plugins such as attenuators, cable equalizers, cable simulators, high tap values, and return path attenuators. If your company wants to use these plugin components, you need to add a a CodedValueDomain as described below. You do not have to add this domain if you do not intend on using components with plugins.

<CodedValueDomain CoaxName="RFConditioningPluginTypes">
		<CodedValueEntry CoaxName="0"  EsriName="0"  DisplayName="None"/>
		<CodedValueEntry CoaxName="20" EsriName="20" DisplayName="CE"/>
		<CodedValueEntry CoaxName="21" EsriName="21" DisplayName="CS"/>
		<CodedValueEntry CoaxName="22" EsriName="22" DisplayName="RA"/>
		<CodedValueEntry CoaxName="23" EsriName="23" DisplayName="HT"/>
		<CodedValueEntry CoaxName="99" EsriName="99" DisplayName="JMP"/>
	</CodedValueDomain>

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?