MM_OBJECT_TYPES Table

Process ArcFM Object Types tool caches object type information about all tables in the current workspace to the MM_OBJECT_TYPES table.

This table is outlined as follows:

Name

Type

Description

OBJECTID

Integer

A unique identifier for a given row in the table.

TABLENAME

String

The fully qualified table name of a given table in a database.

OBJECT_TYPE

Integer

The object type of a given table. This is a value from the MMClassObjectType enum.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?