Troubleshooting
Issue | Resolution/Action |
---|---|
Device does not produce an alarm sound when tested. |
|
Device beeps and Standby LED blinks every 48 s |
Battery may be low or drained. Replace the device. |
Device beeps twice and Standby LED blinks every 48 s |
|
Device produces alarm sound unexpectedly without smoke or steam or high temperature. |
IMPORTANT: After an alarm event, the device that
has blinking Standby LED every 2 s is the triggered device. Identify
the device and follow steps 3 to 5.
|