990-6230-001

Remove the UPS from the Pallet

  1. Move the UPS to the final installation area using a forklift.
  2. Remove the shipping materials from the UPS.
  3. Loosen the bolts and remove the four shipping brackets.
  4. Remove the indicated pallet parts.
  5. Use a forklift to lift the UPS and remove the remaining pallet parts.
  6. Move the UPS to its final location and use a wrench to lower the levelling feet. Ensure that the cabinet is level.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?