Important Safety Instructions — SAVE THESE INSTRUCTIONS
Read these instructions carefully and look at the equipment to become familiar with it before trying to install, operate, service or maintain it. The following safety messages may appear throughout this manual or on the equipment to warn of potential hazards or to call attention to information that clarifies or simplifies a procedure.
DANGER |
|---|
|
DANGER indicates a hazardous situation which, if
not avoided, will result in death or serious injury.
Failure to follow these instructions will result in death or serious injury.
|
WARNING |
|---|
|
WARNING indicates a hazardous situation which,
if not avoided, could result in death or serious injury.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
CAUTION |
|---|
|
CAUTION indicates a hazardous situation which,
if not avoided, could result in minor or moderate injury.
Failure to follow these instructions can result in injury or equipment damage.
|
| NOTICE |
|---|
|
NOTICE is used to address practices not related
to physical injury. The safety alert symbol shall not be used with
this type of safety message.
Failure to follow these instructions can result in equipment damage.
|
Please Note
Electrical equipment should only be installed, operated, serviced, and maintained by qualified personnel. No responsibility is assumed by Schneider Electric for any consequences arising out of the use of this material.
A qualified person is one who has skills and knowledge related to the construction, installation, and operation of electrical equipment and has received safety training to recognize and avoid the hazards involved.
Per IEC 62040-1: "Uninterruptible power systems (UPS) -- Part 1: Safety Requirements," this equipment, including battery access, must be inspected, installed and maintained by a skilled person.
The skilled person is a person with relevant education and experience to enable him or her to perceive risks and to avoid hazards which the equipment can create (reference IEC 62040-1, section 3.102).
Electromagnetic Compatibility
| NOTICE |
|---|
|
Risk of electromagnetic disturbance
This is a product Category C3 according to IEC 62040-2.
This is a product for commercial and industrial applications in the
second environment - installation restrictions or additional measures
may be needed to prevent disturbances. The second environment includes
all commercial, light industry, and industrial locations other than
residential, commercial, and light industrial premises directly connected
without intermediate transformer to a public low-voltage mains supply.
The installation and cabling must follow the electromagnetic compatibility
rules, e.g.:
Failure to follow these instructions can result in equipment damage.
|
Safety Precautions
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Read all instructions in the installation manual before
installing or working on this product.
Failure to follow these instructions will result in death or serious injury.
|
DANGER |
|---|
|
hazard of electric shock, explosion, or arc flash
Do not install the product until all construction work
has been completed and the installation room has been cleaned.
Failure to follow these instructions will result in death or serious injury.
|
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
The product must be installed according to the specifications
and requirements as defined by Schneider Electric. It concerns in
particular the external and internal protections (upstream breakers,
battery breakers, cabling, etc.) and environmental requirements. No
responsibility is assumed by Schneider Electric if these requirements
are not respected.
Failure to follow these instructions will result in death or serious injury.
|
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
The UPS system must be installed according to local and
national regulations. Install the UPS system according to:
Failure to follow these instructions will result in death or serious injury.
|
DANGER |
|---|
|
hazard of electric shock, explosion, or arc flash
Failure to follow these instructions will result in death or serious injury.
|
DANGER |
|---|
|
hazard of electric shock, explosion, or arc flash
The product is not designed for and must therefore not
be installed in the following unusual operating environments:
Failure to follow these instructions will result in death or serious injury.
|
DANGER |
|---|
|
Hazard of electric shock, explosion, or arc flash
Do not drill or cut holes for cables or conduits with
the gland plates installed and do not drill or cut holes in close
proximity to the UPS system.
Failure to follow these instructions will result in death or serious injury.
|
DANGER |
|---|
|
Hazard of electric shock, explosion, or arc flash
Do not make mechanical changes to the product (including
removal of cabinet parts or drilling/cutting of holes) that are not
described in the installation manual.
Failure to follow these instructions will result in death or serious injury.
|
| NOTICE |
|---|
|
risk of overheating
Respect the space requirements around the product and
do not cover the ventilation openings when the product is in operation.
Failure to follow these instructions can result in equipment damage.
|
Electrical Safety
DANGER |
|---|
|
hazard of electric shock, explosion, or arc flash
Failure to follow these instructions will result in death or serious injury.
|
Distribution-Related Backfeed
The upstream disconnection switchgear must be suitable for disconnection purposes. Before working on the upstream supply, the MBB must be locked in the open position using the built-in lockout function.
When installing
the parallel maintenance bypass panel, warning labels must be posted
on the load side of all upstream disconnection devices. The labels
must be supplied by the user, displaying the following text (or equivalent
in a language which is acceptable in the country in which the UPS
system is installed):
DANGER
WARNING
CAUTION
DANGER