990-5913E-001

Prepare for Cables

  1. Open the door(s). On GVSCBC10A2 and GVSCBC10B2, remove two screws to open the left door.
  2. Lockout/Tagout the battery breaker in the OFF (open) position.
  3. Remove the breaker protection plates.

    GVSCBC7C, GVSCBC7D, GVSCBC7E

    GVSCBC10A2, GVSCBC10B2

  4. Remove the kit with copper bars/cables from the classic battery cabinet. Save for interconnection of the batteries – see Connect the Power Cables.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.