990-5912E-001

Connect the Signal Cables for Galaxy VS UPS – Single System

NOTE: Route the signal cables separately from the power cables and route the Class 2/SELV cables separately from the non-Class 2/non-SELV cables.

GVSBPSU10K20H

GVSBPSU20K60H and GVSBPSU80K120H

  1. Connect the Class 2/SELV signal cables for the disconnect device indicator lights from the control terminal block in the maintenance bypass panel to the UPS as per your configuration.
    NOTE: The disconnect device indicator light circuit is considered Class 2/SELV. Class 2/SELV circuits must be isolated from the primary circuitry. Do not connect any circuit to the disconnect device indicator light terminals unless it can be confirmed that the circuit is Class 2/SELV.

    Single System – Single Mains

    Single System – Dual mains

  2. Connect the non-Class 2/non-SELV signal cables from the control terminal block in the maintenance bypass panel to the UPS as per your configuration.

    Single System – Single Mains

    Single System – Dual Mains

  3. Pull up the slack in the signal cables and fasten the signal cables to the cable reliefs.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.