990-66231A-001

UPS Shipping Weights and Dimensions

UPS rating (Commercial reference) Weight kg Height mm Width mm Depth mm
10 kVA (E3SP10KH) 50 813 380 780
15 kVA (E3SP15KH) 51 813 380 780
20 kVA (E3SP20KH) 52 813 380 780
30 kVA (E3SP30KH) 69 970 380 982
40 kVA (E3SP40KH) 73 970 380 982
15 kVA (E3SP15KHIN) 52 813 380 780
20 kVA (E3SP20KHIN) 53 813 380 780
30 kVA (E3SP30KHIN) 70 970 380 982
40 kVA (E3SP40KHIN) 74 970 380 982
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?