About the Document

Document Scope

The aim of this guide is to provide users, installers, and maintenance personnel with the technical information and procedures needed to use and maintain the EcoStruxure™ Panel Server.

Validity Note

This guide applies to the EcoStruxure Panel Server models and firmware versions described in the following table:

Commercial reference Hardware version Firmware version
001.000.000 002.000.000

PAS400

EcoStruxure Panel Server Entry firmware version 002.002.000 or greater for hardware version 001.000.000

PAS600, PAS600T, PAS600L

EcoStruxure Panel Server Universal firmware version 002.002.000 or greater for hardware version 001.000.000

PAS600, PAS600P, PAS600L

EcoStruxure Panel Server Universal firmware version 002.002.000 or greater for hardware version 002.000.000

PAS600LWD, PAS600PWD

EcoStruxure Panel Server Universal Wired by Design model firmware version 002.002.000 or greater for hardware version 002.000.000

PAS800, PAS800L, PAS800P

EcoStruxure Panel Server Advanced firmware version 002.002.000 or greater for hardware version 001.000.000

EcoStruxure Panel Server Advanced firmware version 002.002.000 or greater for hardware version 002.000.000

NOTE: The content of this guide also applies to EcoStruxure Panel Server Wired by Design models PAS600LWD and PAS600PWD. A Wired by Design model is a Panel Server without the capability to connect to IEEE.802.15.4 wireless devices and without Wi-Fi communication capability.

All the information related to the Panel Server presented in this guide applies to Wired by Design models except information about wireless devices and Wi-Fi communication.

Online Information

The characteristics of the products described in this document are intended to match the characteristics that are available on www.se.com. As part of our corporate strategy for constant improvement, we may revise the content over time to enhance clarity and accuracy. If you see a difference between the characteristics in this document and the characteristics on www.se.com, consider www.se.com to contain the latest information.

Product Related Information

WARNING
UNEXPECTED START OF OPERATION
Only allow remote and/or scheduled control of loads for non-critical electrical loads that can safely be left unattended.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

General Cybersecurity Information

In recent years, the growing number of networked machines and production plants has seen a corresponding increase in the potential for cyber threats, such as unauthorized access, data breaches, and operational disruptions. You must, therefore, consider all possible cybersecurity measures to help protect assets and systems against such threats.

To help keep your Schneider Electric products secure and protected, it is in your best interest to implement the cybersecurity best practices as described in the Cybersecurity Best Practices document.

Schneider Electric provides additional information and assistance:

Product Related Cybersecurity Information

WARNING
POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY, AND CONFIDENTIALITY
  • Disable unused ports/services to help minimize pathways for malicious attackers.
  • Place networked devices behind multiple layers of cyber defenses (such as firewalls, network segmentation, and network intrusion detection and protection).
  • Use cybersecurity best practices (for example, least privilege, separation of duties) to help prevent unauthorized exposure, loss, modification of data and logs, or interruption of services.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

For more information about cybersecurity related to the EcoStruxure Panel Server, refer to:

Environmental Data

For product compliance and environmental information, refer to the Schneider Electric Environmental Data Program.

Available Languages of the Document

The document is available in these languages:

Related Documents

Title of documentation

Reference number

EcoStruxure Panel Server - Catalog

PLSED310196EN

EcoStruxure Panel Server Entry - Instruction Sheet

NNZ76760

EcoStruxure Panel Server Universal - Instruction Sheet

GEX84977

EcoStruxure Panel Server Universal Wired by Design  - Instruction Sheet

PKR28607

EcoStruxure Panel Server Advanced - Instruction Sheet

BQT54848

EcoStruxure Panel Server - Wireless Devices / Wi-Fi Antenna - Instruction Sheet

NNZ58425

EcoStruxure Panel Server Entry - Firmware Release Notes

EcoStruxure Panel Server Universal - Firmware Release Notes

EcoStruxure Panel Server Advanced - Firmware Release Notes

EcoStruxure Panel Server - Cybersecurity Guide

EcoStruxure Panel Server - Modbus File

DOCA0241EN

EcoStruxure Panel Server - Alarm File

DOCA0330EN

EcoStruxure Power Commission Mobile Application - User Guide

DOCA0366EN

EcoStruxure Cybersecurity Admin Expert User Guide

CAE_User_Guide

EcoStruxure Power - Guide for Designing and Implementing a Cyber Secure Digital Power System - Technical Guide

ESXP2TG003EN

Wireless Communication Architectures With EcoStruxure Panel Server - Design Guide

DOCA0289EN

You can download these technical publications and other technical information from our website at www.se.com/ww/en/download/.

Information on Non-Inclusive or Insensitive Terminology

As a responsible, inclusive company, Schneider Electric is constantly updating its communications and products that contain non-inclusive or insensitive terminology. However, despite these efforts, our content may still contain terms that are deemed inappropriate by some customers.

Trademarks

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?