Displaying and Publishing Alarms
Consulting Active Alarms
This function is available on Panel Server Entry, Universal, and Advanced.
Active alarms issued by connected devices are displayed on the Panel Server webpages at Monitoring and Control, on the Data page of each device. An active alarm disappears when conditions of the alarm are no longer met.
Alarms are defined by severity:
-
High severity
-
Medium severity
-
Low severity
For information about identifying alarm severity, refer to Alarm Icons.
Publishing Alarms
Active alarms can be published by the following methods, depending on the data publication method selected:
-
Schneider Electric cloud (all models): When the Panel Server is connected to the Schneider Electric cloud, alarms are published to the cloud application. The selection of alarms is managed at the cloud level, and is available for display only at .
-
By email (Advanced model): When the Email service for alarms is activated, email notifications for selected alarms are sent to the recipient list.
-
On the Panel Server webpages at Notifications (Advanced model): Appearance and disappearance of selected alarms are displayed on the Notifications webpage
Selecting Alarms for Notification and Publication by Email (Advanced Model)
For each device connected to the Panel Server Advanced, you can select or deselect the notification and publication by email of alarms issued in the case of electrical events or communication loss. By default, publication of each alarm is deselected.
A maximum of 500 alarms can be selected concurrently. Of the 500 selected alarms, a maximum of 300 can be from Modbus-SL devices.
Alarms to be published in the Notifications page and by email when they become active can be selected individually for each device as follows.
-
Click the device name on the Panel Server webpages, at .
-
Click Alarms. The alarms are displayed in a table with a column indicating the severity. Click the double arrow icon at the top of the column to sort the alarms by severity.
-
Select/deselect an alarm for publication with the Alarm publication checkbox.