Appendix C: Wireless Device Network Indicators

Signal Quality Level

The signal quality level is based on the LQI and PER network indicators, as shown in the following table:

  Link quality indicator (LQI)

LQI < 30

30 ≤ LQI < 60

60 ≤ LQI

Packet error rate (PER)

PER > 30%

Weak

Weak

Fair

10% < PER ≤ 30%

Weak

Fair

Good

PER ≤ 10%

Fair

Good

Excellent

Network Indicators

The following table describes the network indicators of wireless devices.

Information type Description

RSSI

Displays the power level of the wireless signal.

  • 0 to -65 dbm indicates a good power level

  • -65 to -75 dbm indicates an average power level

  • -75 dbm indicates a poor power level with risk of outage

LQI

Displays the measurement of the strength and/or the quality of the received frames.

NOTE: It is recommended to use this indicator as the main indicator of acceptance.

PER

Displays the ratio of the packet that does not reach a destination over the total expected number of packets. It is expressed as a percentage.

The calculation of the PER (packet error rate) indicator depends on the type of indicator:

  • Device indicator: provided by the device.

  • Panel Server indicator: calculated over a 10–minute sliding window, and refreshed every 30 seconds.

  • Link indicator: displays the higher of the two previous indicators.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?