Diagnostics
Presentation
Diagnostics data provides statistical data about the Panel Server and connected devices. The events are gathered by type of application: cloud connection, Modbus Serial network, and wireless network.
Availability
This function is available on Panel Server Entry, Universal, and Advanced.
Setting the Parameters
Diagnostics are set on the Panel Server webpages:-
At
, device diagnostics:
- ,
EcoStruxure Panel Server Diagnostics
Parameter | Description |
---|---|
Ethernet information |
Ethernet information switched port
|
Modbus serial client counter information |
Displays diagnostics counters for Modbus-SL protocol:
Reset counters button allows you to reset the counters to zero. |
Modbus TCP/IP server connection information |
Displays connection information for Modbus TCP/IP protocol:
Reset counters button allows you to reset the counter to zero. |
Modbus TCP server counter information |
Displays message counters for Modbus TCP/IP protocol:
Reset counters button allows you to reset the counters to zero. |
Wireless (802.15.4) identification* |
Displays identification of IEEE 802.15.4 wireless network:
|
Wireless (802.15.4) network status* |
Displays status of the IEEE 802.15.4 wireless network
|
Modbus Devices Diagnostics
Parameter | Description |
---|---|
Modbus information |
Displays identification and diagnostics counters for Modbus devices:
Reset device counters button allows you to reset the device counters to zero. |
The table of channels displays information about Input 1 and Input 2 devices, where relevant.
Wireless Devices Diagnostics
Parameter | Description |
---|---|
Modbus identification* |
Displays Modbus identification:
|
Wireless network indicator* For more information, see Appendix C. |
Displays connection information of the wireless devices:
|
Status | Power source Displays power source of the wireless devices. |
Power source backup* Displays backup power source of the wireless devices, where relevant. |
|
Inputs/output* |
Displays the following information:
|
Embedded Input Device Diagnostics (PAS600L, PAS600LWD and PAS800 Models)
Parameter | Description |
---|---|
Embedded input |
For digital input configured as Pulse counter, displays Raw counter value |
For digital input configured as Standard input, displays Status |
System Monitoring Diagnostics
Parameter | Description |
---|---|
Health state |
Uptime indicates how long the Panel Server has been running for. |
Health state indicates the Panel Server state:
|
|
Global performance |
Displays Panel Server performances:
|