Showing 111 - 120 of 272 results

Page 12 of 28
  • LED indications

    ELKO - Smart Smoke Alarm Battery – Wiser Home Device user guide

    LED indications LED indications LED indications Pairing User Action LED Indication Status Press the Setup/Reset button 3 times Status LED blinks amber, once per second. Pairing mode is active for 30 seconds. When pairing is completed, status LED glows green for some time before turning Off
  • LED indications

    ELKO - Smart Smoke Alarm 230 V – Wiser Home Device user guide

    LED indications LED indications LED indications Pairing User Action LED Indication Status Press the Setup/Reset button 3 times Status LED blinks amber, once per second. Pairing mode is active for 30 seconds. When pairing is completed, status LED glows green for some time before turning Off
  • Setting the start and end time

    ELKO - SmartBlinds Puck – Wiser Home Device user guide

    Setting the start and end time Setting the start and end time Setting the start and end time Using the Wiser Home app, you can define the start and end time of the seasonal comfort mode. To set the start and end time of the seasonal comfort mode: In the Seasonal Comfort Mode set-up page, tap Time
  • Setting the start and end time

    ELKO - SmartBlinds Push – Wiser Home Device user guide

    Setting the start and end time Setting the start and end time Setting the start and end time Using the Wiser Home app, you can define the start and end time of the seasonal comfort mode. To set the start and end time of the seasonal comfort mode: In the Seasonal Comfort Mode set-up page, tap Time
  • ELKO - Power Tag Control Wiser Home Device User Guide

    the detectionof movement by a motion sensor. – Away Mode (Enable or Disable): The Away Mode is intended to set yourHome to a practical state for longer absences, such as leaving for theweekend. NOTE: Maximum 10 conditions can be added. 5. Select a device to set the condition. Then, choose the state
  • Creating an Automation

    Elko Wiser Home – System User Guide (Norway)

    ). Select the type of trigger to activate your automation. Device status change: Choose a specific device whose status change (e.g., on/off, open/closed) will trigger the automation. Away Mode: Enable or disable to trigger automation when you leave or return home. Energy price changes: Trigger an
  • ELKO - Schneider Charge

    www.se.com Tariff Tariff Set tariff in the Wiser Home app to view energy costs and billing information. Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 elko.no/contact www.se.com Charging mode Charging mode Using the Wiser Home app, to manage the mode of
  • Silencing the device

    ELKO - Smart Smoke Alarm 230 V – Wiser Home Device user guide

    Silencing the device Silencing the device Silencing the device Hush the smoke alarms During an alarm event, first identify the smoke alarm/s that detected smoke, these will have Red LEDs blinking. Then short press the Test/Hush button on the smoke alarm to stop the alarm. In hush mode, the smoke
  • Pairing Anti-Tripping Module with Schneider Charge

    ELKO - Schneider Charge – Wiser Home Device User Guide

    Anti-Tripping Module and Schneider Charge is completed as per the installation manual. Do not shut down the power supply during pairing process. https://www.youtube.com/embed/Qfu64Z0amak?loop=1&controls=1 Activate pairing mode Activate pairing mode in Anti-Tripping Module as mentioned below: For
  • Silencing the device

    ELKO - Smart Smoke Alarm Battery – Wiser Home Device user guide

    Silencing the device Silencing the device Silencing the device Hush the smoke alarms During an alarm event, first identify the smoke alarm/s that detected smoke, these will have Red LEDs blinking. Then short press the Test/Hush button on the smoke alarm to stop the alarm. In hush mode, the smoke
Page 12 of 28