DUG_Smart Smoke Alarm Battery_WH-00

Silencing the device

Hush the smoke alarms

During an alarm event, first identify the smoke alarm/s that detected smoke, these will have Red LEDs blinking. Then short press the Test/Hush button on the smoke alarm to stop the alarm.

IMPORTANT: In hush mode, the smoke alarm will not detect smoke/high temperature for 10 minutes. After 10 minutes the smoke alarm resumes to normal operation. During this time, the Standby LED blinks once every 8 s.
  • If smoke is detected while the alarm is in hush mode, high-temperature detection remains active.

  • If high temperature is detected while the alarm is in hush mode, smoke detection remains active.

  • If both smoke and high temperature are detected simultaneously and the alarm is set to hush mode, both detections are disabled for 10 minutes.

  • In interconnected systems, if multiple alarms show blinking red LEDs and are actively alarming, briefly press the Test/Hush button on each device. All alarms will silence within 5 to 10 seconds.

NOTE: Wait for 10 minutes before performing any test to avoid malfunctioning of the smoke alarm. Once the device is set to Hush Mode the status can be checked in Wiser Home app.

Temporarily disabling smoke detection

To temporarily disable the smoke detection of a smoke alarm, short press the Test/Hush button once when the smoke alarm is in Standby mode. The smoke alarm will not detect smoke for 10 minutes. During this mode the Standby LED blinks once every 8 s.

NOTE: The temperature sensor remains active even when the smoke detection is disabled.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.