Showing 241 - 250 of 272 results

Page 25 of 28
  • Testing the device

    ELKO - Smart Smoke Alarm 230 V – Wiser Home Device user guide

    Testing the device Testing the device Testing the device The smoke alarm has a test mode that helps ensure the proper operation. It is recommended to test the smoke alarm once a month. If the smoke alarm is installed in a mobile home, it is recommended to test the smoke alarm weekly and before
  • LED Indications

    ELKO - SmartSensor PIR wireless – Wiser Home Device user guide

    ) → → (3 sec) → Indicates the pairing mode after function key is pressed 3 times within 1 second. If pairing is not successful, the LED is On for 3 seconds and then turns Off. Green LED is On for 3 seconds → (3 sec) → Pairing was successful. If already paired Action LED Indication Status Green LED blinks
  • Using the device

    ELKO - Smart Water Heater Puck – Wiser Home Device User Guide

    switched on, it will start directly. By default, the device will be in manual schedule mode. Wiser Home AI: This feature automatically schedule your loads when the cost is the cheapest. Refer to Wiser Home AI. Customised schedule: You can create your own schedule to turn on or off your device. Refer to
  • Configuring the device

    ELKO - Power Tag Control – Wiser Home Device User Guide

    identify the device. The status LED blinks red and connected lighting devices blinks On/Off, upon successful identification of the dimmer. Tap OK when you finish identifying the device. G Delete: Tap to remove the device from the system. All the historical data will be deleted from the app. If there is a problem while pairing, refer to resetting pairing mode.
  • ELKO - Power Tag Control

    elko.no/contact www.se.com Deleting an automation Deleting an automation Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 elko.no/contact www.se.com Resetting pairing mode Resetting pairing mode If the PowerTag loses connection with the Hub, you can re-enter
  • Adding a Schedule

    Elko Wiser Home – System User Guide (Norway)

    default schedule is created when climate devices are assigned. When signed in as a Professional Installer: In the Device Control Screen, the Follow schedule toggle is Off by default. All rooms are set to Manual mode. You can enable the Follow schedule toggle if you want the default heating schedule to
  • Assigning a shutter group to the Wireless switch

    ELKO - SmartSwitch Push Wireless Plus – Wiser Home Device User Guide

    group and tap Save. If the device is in sleep mode, press the top-right push button on the Wireless switch 3 times to wake up the device. Then tap Confirm in the app to apply the settings. For more information, refer to Wake up the device. Each group can include up to 60 devices. You can create a
  • Device settings

    ELKO - Motion Sensor Outdoor, 360 – Wiser Home Device user guide

    when the ambient brightness falls below the threshold level. 1-2000 Lux : Set the brightness threshold at which the sensor should turn ON the load. When the ambient brightness falls below the set lux level, the motion sensor will be triggered to operate. Day mode : The sensor will turn the load ON
  • Room setting

    ELKO - Smart ZB Thermostat 16 A – Wiser Home Device user guide

    between a room being occupied and then transitioning to an unoccupied state.This delay ensures that the system doesn't immediately switch to an unoccupied mode when a room becomes vacant, preventing unnecessary fluctuations and providing a grace period in case the room becomes occupied again
  • Technical Data

    ELKO - Smart ZB Thermostat 16 A – Wiser Home Device user guide

    Technical Data Technical Data Technical Data Nominal voltage: AC 230 V ~, 50 Hz Maximum current rating Resistive load: max. 16 A, 3520 W Inductive load: max. 4 A Power consumption In standby mode (Psm) : 0.24 W In networked standby (Pnsm) : 0.32 W Networked standby with display (P) : 0.5 W Type of
Page 25 of 28