ELKO - Smart Water Heater Puck_WH_00

Using the device

The Water Heater Control Panel allows you to turn on or off the device and monitor the power consumption.

On the Control tab, tap All devices or a room tab where the Plug is located > Water Heaterto access the control panel.

On the Device Control Screen, you can see the following:

A

Total energy consumption in the session

B

Tap to manually turn the device ON/OFF.

C

Device can be controlled and triggered by a schedule. You can change to any one of the following schedule modes:

  • Manual:

    Device will start when you turn on. If it is already switched on, it will start directly.
    NOTE: By default, the device will be in manual schedule mode.
  • Wiser Home AI: This feature automatically schedule your loads when the cost is the cheapest. Refer to Wiser Home AI.

  • Customised schedule: You can create your own schedule to turn on or off your device. Refer to Creating a schedule topic.

D

You can see the 24 hr schedule for the device based on the electricity rates.

E

You can rename the device or remove the device from the Wiser system, change location, nominal power. Refer to Configuring the device.

F

Add to favourites (F) - Tap to add the device to the Favourite devices section on the Home screen. To know more about Favourite, refer to Managing Favourites in the respective System User Guide..

NOTE:

Similarly you can control and check the current status of Water Heater from Control tab.

  • Tap to turn on/ off the device.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.