Showing 31 - 40 of 387 results

Page 4 of 39
  • Pairing the main device

    ELKO Smart Tag – Wiser Home Device User Guide

    only have single SmartTag in the entire Wiser System, the Control page will not be visible. All functions will be accessible through the Home page. You will be notified to enter the tariff after the SmartTag is commissioned, refer to Setting Tariff If you have already configured your tariff, you will be directed to Home screen to view the status of device.
  • Creating an automation

    ELKO - Smart Plug 16 A – Wiser Home Device User Guide

    Away mode. Energy price changes: To define the energy price limit. This condition is available only if your tariff is set to Peak/Off-Peak or Dynamic. Refer to Setting Tariff. Maximum 10 conditions can be added. To remove an added condition, swipe left and tap . To set a specific time for your
  • Pairing the main device with On Grid solar system

    ELKO Smart Tag – Wiser Home Device User Guide

    direction is correct. If you have selected the option as No, the power direction is Grid to Home. Enable the Reverse Direction toggle switch if the power direction is incorrect. Tap Save. You will be notified to enter the tariff after the SmartTag is commissioned, refer to Setting Tariff. If you
  • ELKO - Smart Water Heater Puck

    /contact www.se.com Setting the device location Setting the device location Using the Wiser Home app, add the module to any room (such as living room, bedroom etc). Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 elko.no/contact www.se.com Changing Nominal
  • Creating an Automation

    Elko Wiser Home – System User Guide (Norway)

    automation based on changes in energy prices. This trigger is available only if your tariff is set to Peak/Off-Peak or Dynamic. Refer to Setting Tariff. The system manages electricity pricing at a precision of 0.01 €/kWh. Example: The daily average electricity price is 0.24 €/kW. You have set your
  • Elko Wiser Home System User Guide (Norway)

    .......................................................................................... 110Support ............................................................................................ 111App Theme ...................................................................................... 112 Setting Tariff
  • ELKO - Schneider Charge

    reducing the power of the load. This keeps the total consumption of the system under a defined limit. The limit value is set by the size of the main incomer switch, refer to Setting Tariff. Devices that are eligible will be added automatically to the Anti-Tripping Management. Schneider Electric 35
  • ELKO Smart Tag Wiser Home Device User Guide

    visible. All functions will be accessible throughthe Home page.NOTE: You will be notified to enter the tariff after the SmartTag iscommissioned, refer to Setting TariffNOTE: If you have already configured your tariff, you will be directed toHome screen to view the status of device. Pairing additional
  • Konfigurering - fastpris

    Elko Wiser Home – Brukerveiledning for systemet (Norge)

    Konfigurering - fastpris Konfigurering - fastpris Konfigurering - fastpris For å stille inn fastpris: Etter å ha lest informasjonen om innføring av tariff. På skjermen Tariff trykker du på Elektrisitet. Hvis du allerede har konfigurert tariffinnstillingene dine, følger du menynavigasjonen hvis du
  • Konfigurering – innmatingstariff

    Elko Wiser Home – Brukerveiledning for systemet (Norge)

    Konfigurering – innmatingstariff Konfigurering – innmatingstariff Konfigurering – innmatingstariff Innmatingsprisen vil kun vises for brukere med strømnettilkoblet solenergianlegg som leverer strøm til nettet. Du vil bli bedt om å oppgi «Feed in Tariff» (innmatingstariff) (FOT) på siden Innsikter
Page 4 of 39