Showing 321 - 330 of 387 results

Page 33 of 39
  • Creating a moment

    ELKO - SmartMove Dimmer Push – Wiser Home Device user guide

    -right screen. After setting all conditions, tap Save. Once the moment is saved, it will appear on the Moments tab. Tap on the moment to enable it. If you want to see the created moments on the Home screen, go to Home > > Home Screen > Moments and enable the Moments toggle switch. You can also rearrange the moments by tapping Edit from the Moments tab on the Home screen, or by tapping Automation > Moments > Reorder.
  • Creating a moment

    ELKO - SmartMove Relay 10A – Wiser Home Device user guide

    actions menu, you can select the devices (C). Once devices are selected, tap Done. On the Moment creator page, tap the device to set the condition. For example, if it is a Motion Sensor Switch: Tap to turn on (D) and tap Set on the top-right screen. After setting all conditions, tap Save. Once the
  • Example of an automation

    ELKO - Wiser 16 A Relay for Temperature Control – Wiser Home Device user guide

    Example of an automation Example of an automation Example of an automation This demonstration guides you through setting up an automation that activates heating to a set temperature of 20 °C when the room temperature drops below 18 °C. To ensure proper heating control, you must create two separate
  • Example of an automation

    ELKO - Wiser Room Thermostat – Wiser Home Device user guide

    Example of an automation Example of an automation Example of an automation This demonstration guides you through setting up an automation that activates heating to a set temperature of 20 °C when the room temperature drops below 18 °C. To ensure proper heating control, you must create two separate
  • LED indications

    ELKO - SmartSocket Double 16 A – Wiser Home Device user guide

    . Setting (Default state) LED Indication Description The Red LED glows. The Red LED glows when the output is switched ON. All the LEDs are OFF. The LEDs are OFF, when the output is OFF. Alarms LED Indication Description Blinking red fast When there is an overload or over-temperature alarm and the device is switched off. Refer to the Troubleshooting to clear the alarms.
  • Using the device

    ELKO - SmartMove Multiwire Dimmer Push – Wiser Home Device user guide

    information, refer to Setting up a schedule. E Tap to add the device to the Favourite devices section on the Home screen. To know more about Favourite, refer to Managing Favourites in the respective System User Guide. F Tap to open the History screen, which displays previously recorded motion detection
  • Using the device

    ELKO - SmartMove Dimmer Push – Wiser Home Device user guide

    information, refer to Setting up a schedule. E Tap to add the device to the Favourite devices section on the Home screen. To know more about Favourite, refer to Managing Favourites in the respective System User Guide. F Tap to open the History screen, which displays previously recorded motion detection
  • Floor sensors settings

    ELKO - Smart ZB Thermostat 16 A – Wiser Home Device user guide

    temperature ranges from -9°C to +9°C and can be adjusted in 0.1°C increments. Tap Save. Floor sensor limit To set the upper and lower temperature limit: On setting page, tap Floor Sensor Upper Limit to set upper temperature limit of the floor sensor and then tap Save. The temperature ranges form 5
  • Device presetting

    ELKO - Smart ZB Thermostat 16 A – Wiser Home Device user guide

    Electrical Underfloor (Without floor limits) 10 P6 Electrical Underfloor (With floor limits) 10 P7 Hydronic Underfloor Floor Control 10 P8 Electrical Underfloor 10 P9 Regulator Mode (output displayed is based on percentage) Floor Control0 ~ 10 (0% ~ 100%) 30 Cycle time: The Cycle Time setting defines the
  • Creating a moment

    ELKO - SmartDim Multiwire Universal LED Push – Wiser Home Device user guide

    -right screen. After setting all conditions, tap Save. Once the moment is saved, it will appear on the Moments tab. Tap on the moment to enable it. If you want to see the created moments on the Home screen, go to Home > > Home Screen > Moments and enable the Moments toggle switch. You can also rearrange the moments by tapping Edit from the Moments tab on the Home screen, or by tapping Automation > Moments > Reorder.
Page 33 of 39