DUG_SmartDim MW Push_WH-01

Creating a moment

  1. On the Home screen, tap .
  2. Go to Moments and then tap to create a moment.
  3. Enter the name of the moment (A).
    TIP: You can choose the cover image that represents your moment by tapping .
  4. Tap Add actions (B) to select the list of devices.
  5. In the Add actions menu, you can select the devices (C).
  6. Once the device are selected, tap Done.
  7. On the Moment creator screen, tap the device to set the condition. For example if it is a dimmer:
    • Tap to turn on (D).
    • Drag the slider bar up/down to increase/decrease the brightness (E) and tap Set on the top-right screen.
  8. After setting all conditions, tap Save.
    Once the moment is saved, it will appear on the Moments tab. Tap on the moment to enable it.
    TIP:
    • If you want to see the created moments on the Home screen, go to Home > > Home Screen > Moments and enable the Moments toggle switch.

    • You can also rearrange the moments by tapping Edit from the Moments tab on the Home screen, or by tapping Automation > Moments > Reorder.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?