Showing 61 - 70 of 272 results

Page 7 of 28
  • Creating an automation

    ELKO Smart Tag – Wiser Home Device User Guide

    any of the following (D): Device status change (Select the device) Away Mode (Enable or Disable) Energy Price changes (To define the energy price limit) This condition is available only if your tariff is set to Peak/Off-Peak or Dynamic. Refer to Setting Tariff Maximum 10 conditions can be added
  • ELKO - Motion Sensor Outdoor, 360 Wiser Home Device user guide

    automation.• Away Mode: To turn OFF the motion sensor and the device connected to it by enabling this mode. When the away mode is triggered, sensitivity ofthe motion sensor turns OFF. TIP: You can enable the motion sensor and the device connected to itby increasing the sensitivity level of the motion
  • ELKO - SmartBlinds Push Wiser Home Device user guide

    opening of a shutter or the detectionof movement by a motion sensor. – Away Mode (Enable or Disable): Away mode can also trigger anautomation to turn on the lights, close the shutter etc. For more informationabout Away Mode, refer to the system user guide. NOTE: Maximum 10 conditions can be added. a
  • ELKO - SmartSensor Door/Win Wireless Wiser Home Device user guide

    : This triggers an action when at least one condition is met. 4. Tap Add conditions and select any of the following (C): – Device status change: Select a device to enable automation.– Away Mode: Enable/Disable away mode to trigger an action. TIP: Away mode can also be used as a trigger to turn off the
  • Eco Mode

    Elko Wiser Home – System User Guide (Norway)

    Eco Mode Eco Mode Eco Mode Eco Mode is a smart feature designed to maximize the efficiency of your heating system. It automatically optimizes the stop time of the heating phase, each time the set temperature changes from a higher to lower value. Eco Mode is a system feature that is either activated
  • Comfort Mode

    Elko Wiser Home – System User Guide (Norway)

    Comfort Mode Comfort Mode Comfort Mode Comfort Mode is a smart feature that helps ensure the set-point temperature is reached by the time the heating is scheduled to turn ON. It enhances thermal comfort by adjusting the setpoint ahead of schedule, ensuring the room reaches the desired temperature
  • Charging mode

    ELKO - Schneider Charge – Wiser Home Device User Guide

    Charging mode Charging mode Charging mode Using the Wiser Home app, to manage the mode of charging. On the Control tab, tap All devices > Schneider Charge. On the device control panel page, tap Charging Mode. On the EV Charging Mode menu, select one of the following: Manual: To initiate the
  • Boost Mode

    Elko Wiser Home – System User Guide (Norway)

    Boost Mode Boost Mode Boost Mode Boost Mode will apply a boost of +2 °C for one hour to every room in the system. On the Automation Screen: Tap Boost All. To end boost mode earlier, tap Cancel all overrides.
  • ELKO - SmartBlinds Puck Wiser Home Device user guide

    conditions Start by adding a condition that will triggeryour automation. B A DUG_SmartBlinds Puck_WH-00 49 ELKO - Smart Blinds Puck 5. Tap Add conditions and select any of the following (C): – Device status change: Select a device to enable automation.– Away Mode: Enable / Disable away mode to trigger an
  • ELKO - SmartMove Dimmer Push

    device using app Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France elko.no/contact www.se.com Adjusting the brightness level using app Adjusting the brightness level using app Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France elko.no/contact www.se.com Away Mode Away
Page 7 of 28