ELKO Schneider Charge_WH_00

Charging mode

Using the Wiser Home app, to manage the mode of charging.

  1. On the Control tab, tap All devices > Schneider Charge.

  2. On the device control panel page, tap Charging Mode.

  3. On the EV Charging Mode menu, select one of the following:

    1. Manual: To initiate the charging process immediately after being plugged into an electric vehicle.

    2. Wiser Home AI: To automatically initiate charging during the next available cost-effective slot, based on tariff details.

      IMPORTANT: This feature is applicable only when there are suitable tariffs created. Refer to Wiser Home AI and Tariff plan configuration.
    3. Customized Schedule: To create your own schedule for charging.
      Refer to Creating a schedule.

    NOTE:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.