Showing 71 - 80 of 272 results

Page 8 of 28
  • ELKO - SmartSocket Single 16 A Wiser Home Device user guide

    change (Select the device): An automation will be triggeredbased on a device status, such as the opening of a shutter or the detectionof movement by a motion sensor. – Away Mode (Enable or Disable): Away mode can also trigger anautomation to turn on the lights, close the shutter etc. For more
  • ELKO - SmartDim Multiwire Universal LED Push Wiser Home Device user guide

    of a shutter or the detectionof movement by a motion sensor. – Away Mode (Enable or Disable): Away mode can also trigger anautomation to turn on the lights, close the shutter etc. Refer to the AwayMode topic in the respective System User Guide. NOTE: Maximum 10 conditions can be added. a. In this
  • ELKO - Wiser 16 A Relay for Temperature Control Wiser Home Device user guide

    Temperature Control_WH-00 Wiser 16 A Relay for Temperature Control 4. Tap Add conditions and select any of the following (C): – Device status change: Select a device to enable automation.– Away Mode: Enable/Disable away mode to trigger an action. TIP: Away mode can also be used as a trigger to turn
  • Setting Dimming Mode

    ELKO - SmartDim LED Puck Multiwire – Wiser Home Device User Guide

    Setting Dimming Mode Setting Dimming Mode Setting Dimming Mode Using the Wiser Home app, you can manage the Dimmer modes and settings. On the Home screen, tap . Tap Devices > Micromodule Dimmer > Dimming Mode (A) and select either of the following options and tap Done. RC Mode: When different
  • ELKO - SmartSensor Climate Wireless Wiser Home Device user guide

    action only when all conditions are met.– Any condition: This triggers an action when at least one condition is met. 4. Tap Add conditions and select any of the following (C): – Device status change: Select a device to enable automation.– Away Mode: Enable/Disable away mode to trigger an action. TIP
  • ELKO - SmartMove Relay 10A

    /Off device using app Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France elko.no/contact www.se.com Away Mode Away Mode Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France elko.no/contact www.se.com Voice control Voice control Using Amazon Alexa™ or Google Home
  • Resetting pairing mode

    ELKO - Power Tag Control – Wiser Home Device User Guide

    Resetting pairing mode Resetting pairing mode Resetting pairing mode If the PowerTag loses connection with the Hub, you can re-enter pairing mode to commission it to the Wiser system. When the PowerTag Control LED blinks red, it indicates a loss of communication between the Wiser Hub and the
  • Seasonal Comfort Mode

    Elko Wiser Home – System User Guide (Norway)

    Seasonal Comfort Mode Seasonal Comfort Mode Seasonal Comfort Mode If you have a shutter control devices installed at your home, Seasonal Comfort Mode feature will be available. Seasonal Comfort Mode is a smart feature helps maintain the perfect temperature throughout the year by automatically
  • ELKO - SmartSensor Leakage Wireless Wiser Home Device user guide

    triggers an action only when all conditions are met.– Any condition: This triggers an action when at least one condition is met. 4. Tap Add conditions and select any of the following (C): – Device status change: Select a device to enable automation.– Away Mode: Enable / Disable away mode to trigger an
  • Seasonal Comfort Mode

    ELKO - SmartBlinds Puck – Wiser Home Device user guide

    Seasonal Comfort Mode Seasonal Comfort Mode Seasonal Comfort Mode The seasonal comfort mode uses the predicted temperature of a location or information from the light and temperature sensors to determine the temperature of a room and maintain a desired temperature in it by opening or closing the
Page 8 of 28