DUG_PowerTag Control_ELKO_WH-00

Resetting pairing mode

If the PowerTag loses connection with the Hub, you can re-enter pairing mode to commission it to the Wiser system.

  1. When the PowerTag Control LED blinks red, it indicates a loss of communication between the Wiser Hub and the PowerTag Control, wait for 4 min until the LED blinks red several times a second.

    NOTE: If an occasional loss of communication is observed, the LED blink red 1 time.
  2. Then press the PowerTag setup button for > 10 s to reset the device.


After reset, the status LED blinks amber. PowerTag enters pairing mode.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?