DOCA0371EN-00

Product Defense in Depth

It is advised to implement a layered network approach incorporating multiple security and defence controls in your IT and control system to minimize data protection gaps, mitigate single points of failure, and establish a robust cybersecurity posture. The greater the number of security layers within your network, the more challenging it becomes to breach defences, compromise digital assets, or cause disruptions. All communicating equipment's access should be restricted to authorized staff only (using locked enclosures and locked technical room).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?