ESXP2GE019EN-05

Digital Architecture

The digital architecture of the Advanced Protection and Automation application involves collecting the input data from the different products, either directly over Ethernet or via gateways. Ethernet-based communication is required for high-performance network reconfiguration response time.

This data is then used by the Edge Control layer which consists of a set of software-defined applications across the following levels:

  • Operations: EcoStruxure Power Operation (HMI) and EcoStruxure Power Automation System Gateway

  • Maintenance: EcoStruxure Power Automation System Engineering and System Management.

As an option, data from EcoStruxure Power Operation or EcoStruxure Power Automation System Gateway can be passed on to the EcoStruxure Asset Advisor* platform and interpreted by experts as part of the EcoStruxure Service Plan.

The recommended digital architecture for the application is shown below:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?