ESXP2GE002EN-05

Outputs

Outputs are displayed remotely via EcoStruxure Power Monitoring Expert or Power Operation except in specific cases.

The following outputs, when used as part of an energy management plan, can help meet relevant requirements for energy efficiency compliance standards such as ISO 50001, ISO 50002 and ISO 50006.

See the Energy Efficiency Compliance application for detailed information.

Events and Alarms

In EcoStruxure Power Monitoring Expert, smart setpoints provide threshold-based alarming of historical energy usage.

Trends

  • Energy Usage trending

  • All input data detailed above can be displayed as trends.

Dashboards

All dashboards can be configured to run automatically in slide show mode to perform the function of an Energy Kiosk.

Generic data display dashboards can be used:

  • To analyze energy consumption parameters by day of the week, hour of the day, season, etc

  • To compare different energy consumption parameters between buildings, areas or departments, and load types

  • To detect increasing energy consumption caused by deteriorating equipment

Energy usage gadgets *

The following gadgets make it easier to display and interpret energy consumption data:

  • Heat map gadget

    Creates a graphical representation of data where the individual values are represented as colors in a matrix format. This gadget can be used with consumption data to identify usage patterns and anomalies.

  • Consumption / aggregated consumption ranking gadget

    Compares the consumption of loads during specific time intervals, for example by hour, by day of week, or by day.

  • Sankey gadget

    • Shows a flow diagram in which the width of the arrows is proportional to the data values. The diagram starts as a combined flow for all the selected loads and then breaks out into individual flows for each consumer.

    • Used to show WAGES consumption broken down by load type or to visualize consumption costs by load. It can also be used to show power losses.

  • Pareto / aggregated pareto chart gadget

    • Used to perform an 80/20 analysis, identifying the loads that together make up the largest portion, or 80% of the overall consumption

    • Shows consumption data by load for multiple loads, over a selected time period. The information is shown in a combined column and line chart, grouped by aggregation period. The columns are arranged from highest consumption to lowest consumption with a target threshold.

    • Includes a cumulative curve based on the aggregation period consumption values.

Reports

The following reports can be displayed or automatically sent by email:

Energy Management Reports:

  • Energy Usage Report

    Highlights discrepancies and provides a visual interpretation of energy consumption data.

  • Energy Usage by Time of Use Report

    Compares consumption for different time of use periods (on-peak vs off-peak vs partial-peak).

  • Calendar Trend Report

    Provides a monthly or weekly interpretation of hourly usage data, benchmarks performance targets, and identifies peak and off-peak usage patterns

  • Load Profile Report

    Creates a graphical representation of demand or load levels over a period of time. The profile shows peak loads as points on the graph where peak electricity demand is high. A load trend report can be used to analyze the electrical loads at the time of maximum demand.

    This information can show opportunities for developing strategies to improve energy management.

  • Energy Usage by Shift Report

    Compares a measurement from multiple devices for specified time periods (or shifts). This enables energy consumption comparison between shifts (for example, 6:00-1:00 vs. 1:00 to 8:00).

  • Consumption Ranking Report

    Highlights the relative ranking of energy consumption for several loads or areas. Consumption data can be normalized to facilitate the comparison. This report is intended to assist in building energy awareness through relative visualization.

  • Energy Comparison Report

    Compares energy consumption by process, equipment, or area.

  • Energy Cost Report

    Converts energy consumption into cost by applying the relevant tariffs.

  • Energy Period Over Period Report

    Shows consumption data for the same measurement for two different viewing periods side-by-side.

Notifications*

SMS or email notifications are sent on pre-alarm and alarm conditions described above to enable fast action.

Cloud-Based Analytics and Services

As an option, EcoStruxure Service Plan powered by EcoStruxure Power Advisor provides data quality analytics with recommendations from our Schneider Electric service experts.

For further information, refer to Data Quality Management.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.