ESXP2GE023EN-05

Data Processing

Specialized dashboards and dedicated reporting engine analyze data to:

  • Provide highlights on energy consumption according to the most relevant criteria.(per load type, per process line, per area, etc.)

  • Assess energy usage by process area or by product output

  • Highlight what factors (process state, external conditions, etc.) contribute most to energy usage

Energy data processing is embedded in EcoStruxure Power Monitoring Expert or Power Operation.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?