ESXP2GE023EN-05

Outputs

Display of outputs is performed by EcoStruxure Power Monitoring Expert or Power Operation except in specified cases.

The following outputs, when used as part of an energy management program, can help normalize energy data with respect to business operations (number of items produced, etc.) that drive energy usage.

Events and Alarms

In EcoStruxure Power Monitoring Expert smart setpoints offer threshold-based alarming on energy usage.

Trends

Energy Usage Trending

All input data detailed above can be displayed as trends.

Dashboards

All dashboards can be configured to run automatically in slide show mode to perform the function of an Energy Kiosk.

Key Performance Indicator Dashboards*

Dashboards to visualize, analyze, and communicate information about an organization's energy performance KPIs for continuous energy improvement

Reports

The following reports can be displayed or automatically sent by email:

Energy Management Reports:

  • Energy Usage by Shift

    Compares a measurement from multiple devices for specified time periods (or shifts). This means energy usage can be compared between shifts (for example, 6:00 to 1:00 vs. 1:00 to 8:00).

Energy Analysis Reports:*

  • Power Usage per State Report

    Details power usage per state of operation of a machine or process.

  • Energy Consumption per State Report

    Details energy consumption per state of operation of a machine or process.

  • Duration Curve Report

    Shows distribution of power consumption versus duration to detect potential capacity or utilization issues.

  • KPI Engine Report

    Calculates complex energy KPIs.

  • Power Usage Effectiveness (PUE) Report (for data centers)

    Displays and analyzes Power Usage Effectiveness by day, week, month and year.

    Compares the IT loads and support loads.

  • Multi-equipment Operation Report

    Compares duration per state, per machine or process.

  • Single Equipment Operation Report

    Compares duration per state for a single machine or process.

Usage Trending Reports:

  • Multi Device Usage Report

    Displays consumption information for multiple devices.

    View energy usage for a single period, or compare two periods, for example, this month versus last month.

  • Single Device Usage Report

    Displays energy information for one device.

    View energy usage for a single period, or compare two periods, for example, this month versus last month.

Cloud-Based Analytics and Services

As an option, EcoStruxure Service Plan powered by EcoStruxure Power Advisor provides data quality analytics with recommendations from our Schneider Electric service experts.

For further information, refer to Data Quality Management.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?