ESXP2GE020EN-05

Controls

To constantly optimize the power supply strategy, EcoStruxure Microgrid Operation Controller will control field devices dynamically.

Power Controls

The following power controls can be sent:

  • Open/close circuit breakers and transfer switches

  • Adjust/curtail photovoltaic output

  • Charge/discharge batteries

  • Start/stop generator(s)

  • Modify device protection and grounding settings

Building Management System (BMS) Controls

EcoStruxure Microgrid Operation Controller can also interact with the BMS to optimize the overall site energy consumption strategy:

  • Modify HVAC setpoints

Battery Energy Storage System (BESS) Controls (including electrical vehicle)

EcoStruxure Microgrid Operation Controller can send commands to the storage system to optimize its control strategy:

  • When to charge

  • When to discharge

  • Stop charging according to maximum State of Charge

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?