ESXP2GE005EN-05

Outputs

The outputs of the ETAP Simulation Engine are displayed in EcoStruxure Power Operation.

Real-time Dynamic Simulation

Electrical SCADA utilizes data generated by ETAP Simulation Engine to mimic a multitude of user-defined real-case scenarios. It helps to provide an advanced and cost-effective training environment, that prepares operators to quickly respond to various power systems events and emergency situations.

Live Data Display

The live status of the electrical distribution can be represented in the Edge Control software (EcoStruxure Power Operation) in various forms such as:

  • Digital single-line diagrams, with real-time animation of the status of the electrical network

  • Real-time electrical data and equipment status

Reports

In addition to specialized reports, action summary reports are generated to evaluate the steps taken by operators, and to assess and/or validate their competence level.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?