ESXP2GE017EN-05

Inputs

The following data is required:

Data from Active Harmonic Filters (PowerLogic AccuSine PCS+/PCSn/EVC+/PFV+)

Electrical and environmental measurements

  • Voltage, current, frequency

  • Load harmonics, output harmonics

  • Load reactive power, output reactive power

  • Ambient temperature

  • Total harmonic distortion (THD), individual harmonics

Operating mode

  • Operating status, load balance, harmonic correction

  • Reactive, auto start, auto detect modes

Maintenance indicators and alerts

For example: overloads, capacity alarms, required servicing alarm, etc.

Data from UPS (Galaxy VX/VL/VM/VS)

Electrical measurements

  • Input and output voltages, currents, and frequencies

  • UPS active and apparent power

Operating mode

  • Load protected mode

  • Bypass enabled mode

  • Charging mode

  • Test mode

  • UPS in backup mode

Diagnostics measurements

  • Load capacity percentage, output overload

  • Remaining backup time (minutes)

  • Battery temperature, charge level, low battery status, end of life

Data from Surge Protective Devices (ASCO SPD with ASM)*

Electrical and environmental measurements

  • Voltage

  • Frequency

  • Harmonics

System events

  • Surge count

  • Voltage sag/swell count

Maintenance indicators

  • MOV (Metal Oxide Varistor) health

  • SPD health

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?