Context of Application
Arc flash incidents can occur as a result of maintenance activities, human error, or equipment failure. Often, this results in costly downtime, interruption of processes and equipment, and injury to persons. Most standard protective devices do not have the ability to respond quickly to arc flash incidents and to limit their effects on equipment and people.
https://blog.se.com/electrical-safety/2018/08/25/stopping-electrical-fires-using-arc-flash-and-arc-fault-protection/
When not stopped or detected in time, these small arcs, at the final distribution
level, can result in fires, putting lives and installations at risk. To learn more
about Active Arc Fault Detection Devices, check out these links:
https://www.se.com/ww/en/download/document/CA9SS100E/
https://www.se.com/ww/en/download/document/CA9SS099E/
Problem to Solve
The facility manager needs to:
-
Avoid personal injury due to arc flash events.
-
Eliminate or minimize costs resulting from arc flash damage: downtime, repair time, and interruption of processes and equipment.
-
Improve arc flash awareness, enabling fast response of maintenance teams.
-
Provide post arc flash event analysis.
-
Comply with industry requirements for electrical safety in the workplace such as NFPA 70E.
Purpose of the Application
Enhance passive arc flash mitigation solutions
-
By minimizing equipment damage, downtime, and likelihood of personal injury or death through the detection of light and/or current resulting from arc flash events and ultra-fast operation (less than 30 ms) of associated protective devices.
-
By reducing some of the risk during maintenance operation. Energy Reduction Maintenance Settings (ERMS) can be used to help protect staff, occupants, and equipment by temporarily changing circuit breakers to instantaneous trip mode.
Improve maintenance team awareness
By providing the appropriate information to help troubleshoot and identify the root cause of arc flash events. Arc flash incidents are displayed within easy-to-interpret single-line diagrams and graphical incident timelines.
Enable arc flash post incident analysis
By leveraging relevant data. Reported events and alarms are collected from arc flash protective relays.