0100DB2306

Outputs

The output display is performed locally by an Iso-Gard Line Isolation Monitor (LIM) or Iso-Gard Remote Indicator IG2000CBM for instant access by staff. Remote display and additional features are available with the Edge Control software EcoStruxure Power Monitoring Expert or Power Operation.

Live Data Display

The following data is available natively:

  • Insulation monitoring status (color code according to NFPA 99)

  • Insulation integrity absolute value (mA)

Default Isolated Panel diagrams are available with the Insulation Monitoring Module.

Events and Alarms

The following alarms can be raised by the Iso-Gard Line Isolation Monitor (LIM) and EDS461:

  • Insulation fault alarm (visual and acoustic in operating rooms)

  • Insulation fault alarm through communications and dry contact relay, plus visual and acoustic in operating rooms

  • Insulation fault location (per feeder / group of sockets)

  • Transformer fault

Alarms can be raised by the various HMIs (Iso-Gard Line Isolation Monitor (LIM) or Iso-Gard Remote Indicator IG2000CBM) and remotely by the Edge Control software.

Trends

Any Insulation Monitoring parameter such as insulation integrity (mA) can be displayed as a trend in the Edge Control software.

Notifications

  • SMS and/or email notifications can be sent for fast analysis and action.

  • Additional email notifications are available to send reports and other non-critical information.

Reports*

The following report can be displayed or automatically sent via email with the optional Insulation Monitoring module:

Isolated power report

For each Iso-Gard Line Isolation Monitor (LIM) in the room, the report shows:

  • Impedance graph: displays a comparison of impedance measurements to the impedance threshold .The impedance threshold is a blue line and actual measurements are shown as a green line. A red line shows the time when the impedance exceeded the threshold.

  • Events table: shows information for each event that occurred in the date range.

  • Data log table (optional): contains measurements for impedance, load, and temperature in the selected date range. Red values indicate measurements over the limit.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.