0100DB2315

Digital Architecture

The digital architecture of the Power Quality Monitoring and Compliance application recommends direct Ethernet connections to power quality measurement connected products. Data is captured on board connected products and uploaded into the Edge Control software (EcoStruxure Power Monitoring Expert or Power Operation) for data processing, visualization, and reporting.

As an option, data from EcoStruxure Power Monitoring Expert or Power Operation can be passed on to the EcoStruxure Power Advisor platform and interpreted by experts as part of the EcoStruxure Service Plan.

The recommended digital architecture for the application is shown below:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?