0100DB2317

Context of Application

Facility managers of large and critical buildings expect a reliable power network to maximize uptime for their business. However, a number of factors make this more complex. Growing grid instability due to increasing power demand and unpredictable, powerful storms are impacting continuous power availability.

To maximize availability and reliability of their power networks, they require smart and cost-effective remote control, automatic transfer systems, and load management.

Problem to Solve

The facility manager needs to:

  • Remotely control electrical loads from a SCADA system.

  • Automate transfer schemes, load shifting, or simple load shedding operations.

  • Visualize and audit sequences of operations.

Purpose of the Application

Remotely control, visualize, and supervise automatic transfer schemes

A combination of connected hardware and Edge Control software allows for remote controls or monitoring of automated controls.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?