ETE-UM02-00

Connecting to the Website

  1. On a phone, laptop, or tablet, go to Ecostruxure Transformer Expert Install-Check and enter the seven-digit log-on ID, to check the status of the sensor through the website.

    NOTE: After mounting the sensor on the transformer, you cannot read the ID.
  2. The Ecostruxure Transformer Expert Install-Check website confirms if the unit has successfully uploaded and displays the initial temperature and moisture readings from the sensor.

    NOTE: The record lasts for an hour after the upload has occurred.
  3. If the installation is successful, data is available on the Schneider Electric website Ecostruxure Transformer Expert Install-Check within 30 hours of powering the ETE Sensor.

  4. Authorized users receive an email containing their account information, which can be used to login and view data pertaining to the transformer.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?